- Published Oct 10, 2024
- Last Modified Nov 13, 2025
- 13 min
Understanding RCBOs for Electrical Safety
Selecting the right Residual Current Circuit Breaker with Overcurrent Protection (RCBO) involves understanding its features, specifications, and practical installation considerations. This guide covers everything from the meaning of the term, how it works, and its importance in providing robust electrical safety for residential and commercial installations.

What is a Residual Current Circuit Breaker with Overcurrent Protection (RCBO)?
In the realm of electrical safety, Residual Current Circuit Breakers with Overcurrent Protection (RCBOs) play a crucial role in protecting both people and property from electrical hazards. An RCBO combines the functionalities of a Residual Current Device (RCD) and a Miniature Circuit Breaker (MCB) into one compact unit. This integration allows for effective monitoring and rapid disconnection of electricity in the event of faults, such as earth leakage or overloads, thereby preventing serious electric shocks and potential fire hazards.
The primary functions of RCBOs include:
- Protection Against Earth Faults: RCBOs detect imbalances in the electrical current, which can indicate a fault, such as an accidental short circuit or leakage. If such an imbalance is detected, the RCBO will trip and disconnect the circuit almost instantly, minimizing risks to users.
- Overcurrent Protection: In addition to detecting earth faults, RCBOs also provide protection against overcurrent situations—these occur when the current exceeds safe levels due to overload or short circuits. The device will automatically cut off the power supply to prevent overheating and potential damage to electrical appliances.
- Localized Circuit Protection: It is recommended to install an RCBO for each separate circuit in a home or commercial establishment. This ensures that a fault in one circuit does not affect others, allowing for safer and more efficient electrical management.
How Does an RCBO Work?
An RCBO, or Residual Current Circuit Breaker with Overcurrent Protection, is a vital safety device in electrical systems, designed to protect both people and property from two significant types of electrical faults: earth leakage and overcurrent.
The first type of fault that an RCBO protects against is earth leakage, which occurs when there is an unintended break in the electrical circuit. This can happen due to various reasons, such as faulty wiring, insulation damage, or accidents during DIY projects, like accidentally cutting through a cable while using power tools. If the electricity supply is not interrupted during such a fault, it can lead to potentially fatal electric shocks for anyone in contact with the faulty circuit.
When an imbalance in current flow is detected, the RCBO reacts swiftly by disconnecting the circuit. This rapid response is crucial in preventing serious injuries and ensuring safety in residential and commercial settings.
The second type of fault is overcurrent, which can manifest as either an overload or a short circuit. An overload occurs when too many electrical devices draw power from a single circuit, exceeding its capacity. Conversely, a short circuit happens when there is insufficient resistance within the circuit, leading to a sudden surge in current flow that can cause severe damage.
- Overload: This situation arises when the cumulative load on a circuit surpasses its rated capacity, potentially leading to overheating and equipment damage.
- Short Circuit: This represents a more dangerous scenario where a direct connection between live wires occurs, resulting in extremely high current levels that can cause fires or equipment failure.
RCBOs are engineered to monitor current levels continuously and will trip to interrupt the power supply if they detect either an overload or short circuit condition. This dual functionality makes them essential components for comprehensive electrical safety.
Have a look at the RCBO varieties available from different brands below:
Schneider Electric
Functions :
- Protection against short-circuits and cable overloads
- Protection of persons against electric shock by direct contact (10, 30 mA sensitivities)
- Protection of persons against electric shock by indirect contact (100 mA sensitivity)
- Protection of equipment against fires set by leakage currents (100 mA sensitivity)
How RCBOs Differ from RCDs, RCCBs, and MCBs
To fully grasp the meaning of an RCBO, it’s helpful to learn how this versatile device compares to other common electrical safety components, including Residual Current Devices (RCDs), Residual Current Circuit Breakers (RCCBs), and Miniature Circuit Breakers (MCBs).
RCDs vs RCBOs
RCDs are safety devices specifically engineered to protect against electric shocks and electrical fires caused by current leakage. They continuously monitor the flow of electricity through live and neutral wires. If an imbalance is detected, indicating that some current is leaking to the ground, the RCD will automatically disconnect the power supply, often within milliseconds. This rapid response is vital for preventing potentially fatal electric shocks.
Primary functions of RCDs include:
- Leakage Current Detection: RCDs can detect leakage currents as low as 30mA, providing a high level of protection against electrocution.
- Continuous Monitoring: These devices monitor current levels flowing in both directions, ensuring that any discrepancies trigger an immediate trip.
- Test Functionality: All RCDs are equipped with a test button that simulates a fault condition. If the device fails to trip during this test, it indicates a malfunction and requires replacement.
However, it’s important to note that RCDs do not provide protection against overcurrents or short circuits. Their standard ratings typically range from 32A to 64A, corresponding to the internal contact mechanisms. If the current exceeds this rating, the RCD will not trip, which is a limitation compared to RCBOs.
Key differences between RCDs and RCBOs in terms of functionality:
- RCDs are primarily designed to protect against earth leakage currents. They monitor the current flowing through a circuit and trip when they detect an imbalance, indicating that some current is leaking to the ground. This rapid disconnection helps prevent electric shocks and fires. RCDs are suitable for basic protection against electric shocks and are often used in residential settings where simplicity is key.
- RCBOs, on the other hand, combine the functionalities of both an RCD and a Miniature Circuit Breaker (MCB). They provide protection against both earth leakage and overcurrent conditions (which include overloads and short circuits). This dual functionality makes RCBOs more versatile in protecting electrical circuits. RCBOs are particularly valuable in commercial or industrial applications where precise circuit protection is crucial.
RCCBs vs RCBOs
Residual Current Circuit Breakers (RCCBs) are a critical line of defense against electrical hazards. They are designed primarily for earth leakage protection, continuously monitoring the flow of electricity to detect any imbalance. This rapid response helps prevent electrocution and reduces the risk of electrical fires.
- Functionality: RCCBs continuously monitor current levels and will trip when they detect a difference, typically as low as 30mA. However, they do not provide protection against overcurrent conditions such as overloads or short circuits.
- External Protection Requirement: To safeguard against overcurrents, RCCBs must be used in conjunction with external circuit breakers like Miniature Circuit Breakers (MCBs) or Molded Case Circuit Breakers (MCCBs). This requirement can increase installation complexity and space requirements in electrical panels.
When deciding between an RCCB and an RCBO, consider the specific requirements of your electrical system. RCCBs are effective for providing earth leakage protection, but for complete safety, you’ll need a separate circuit breaker to handle overload and short circuit protection.
On the other hand, RCBOs offer an all-in-one solution, which also means they offer protection from both earth leakage and overcurrent conditions. At the same time, they are more versatile and space-efficient for electrical installations.
MCBs vs RCBOs
Miniature Circuit Breakers or MCBs are automatic switches designed to protect electrical circuits from damage caused by overcurrent, which can occur due to overloads or short circuits. When the current exceeds a predetermined level, the MCB will automatically trip, interrupting the flow of electricity and preventing potential damage to wiring and connected devices.
- Functionality: MCBs utilize thermal and magnetic mechanisms to detect faults. The thermal mechanism responds to prolonged overloads, while the magnetic mechanism reacts instantly to short circuits.
- Limitations: One significant limitation of various types of MCBs is that they do not provide protection against earth leakage. This means that while they can prevent circuit damage from excessive current, they cannot safeguard against electric shocks caused by current leaking to the ground.
- Applications: MCBs are commonly used in residential and commercial settings for general circuit protection, such as lighting circuits, air conditioning units, and other household appliances.
The main difference between an MCB and an RCBO (Residual Current Breaker with Overcurrent Protection) lies in the protection they offer. While an MCB provides only overcurrent protection, an RCBO combines both overcurrent protection (for overloads and short circuits) and earth leakage protection, which prevents electric shocks by disconnecting the circuit if it detects leakage current. When selecting between these devices, consider your specific needs for safety and functionality in your electrical installations.
Replacing an MCB with an RCBO
When considering replacing an MCB with an RCBO, it's important to follow proper electrical installation guidelines:
- Regulatory Compliance: In most cases, notification is not required under building control or Part P regulations if the cable sizes are appropriate for the breaker’s rating.
- Qualified Installation: The replacement must be performed by a qualified electrician who adheres to manufacturer instructions and standards outlined in the BS7671 regulations.
- Installation Steps:
- Isolate the electrical supply from the consumer unit.
- Detach the front cover by turning the two fasteners 90 degrees.
- Loosen the bottom terminal of the device carefully.
- Open the bottom device clip.
- Position the RCBO onto the DIN rail and busbar.
- Close the bottom device clip securely.
- Tighten the lower terminal screw firmly.
- Check all cable connections for tightness.
How to Wire RCBOs
Wiring an RCBO (Residual Current Circuit Breaker with Overcurrent Protection) is a critical step in ensuring electrical safety in residential and commercial installations. Before starting the wiring process, it is essential to disconnect the power supply to prevent any risk of electric shock. Here’s a step-by-step guide on how to properly wire an RCBO:
- Disconnect Power Supply: Always ensure that the main power supply is turned off at the consumer unit or distribution board to avoid any accidents.
- Connect Earth Cable: Attach the protective earth (PE) cable to the earth bar within the distribution board. This connection is vital for safety, as it provides a path for fault currents.
- Connect Power Cables: The incoming power cables should be connected to the top terminals of the RCBO. The live (phase) cable, typically brown, should be positioned on the left terminal, while the neutral cable, usually blue, should be connected to the right terminal.
- Prepare and Cut Busbar: If necessary, cut the busbar to the appropriate length before connecting it to the bottom terminals of both the isolator and the RCBO.
- Connect Neutral Cable: A neutral cable should run from the bottom of the isolator to the neutral busbar. Ensure that this connection is secure.
- Outbound Cables: Use twin core and earth cables for outgoing connections. Ensure that earth sleeving is applied to cover all earth wire parts before they are connected to the earth bar.
- Final Connections: Attach the brown live wire to the terminal labeled ‘L’ out and connect the blue neutral wire to 'N' out on the RCBO. Make sure all wiring is cut to appropriate lengths for a neat installation.
- Check Connections: After all connections are made, double-check that everything is secure and correctly positioned before restoring power.
How to Fit RCBOs
Installing an RCBO requires careful attention to detail and adherence to safety standards. Here’s how you can fit an RCBO effectively:
- Select Appropriate RCBO Specifications: Before installation, ensure that your RCBO meets safety standards, look for at least 10mA protection, a current rating of 25A, SRIM certification, and A-type protection for various applications.
- Gather Necessary Tools: You will need a suitable screwdriver for securing connections and a test pen to confirm that power is completely disconnected from the mains supply before you start working.
- Access Wiring: Ensure you have ready access to both live and neutral wiring in your distribution board. This will facilitate easy connections during installation.
- Connect Wiring Securely: Attach the live wire (brown) from your circuit to the appropriate terminal on the RCBO, ensuring it is tightened securely with a screwdriver. Repeat this process for the neutral wire (blue).
- Connect Earth Wire: The earth wire from the RCBO should be connected securely to the earth bar in your distribution board, again tightening it with a screwdriver.
- Power Restoration: Once all connections are made, restore power to the RCBO and any connected equipment carefully.
- Test Functionality: To ensure proper installation, press the test button on the RCBO. The device should trip, confirming that it functions correctly and provides adequate protection against electrical faults.
- Final Checks: After testing, perform a final inspection of all connections and ensure that everything is secure before closing up your distribution board.
According to the Philippine Electrical Code (PEC), all electrical work must be performed by or under the direct supervision of a licensed electrical practitioner. Furthermore, the Republic Act 7920 states that attempting to perform electrical work without the proper license can lead to serious legal penalties, including fines and imprisonment for a period of not less than six months. As such, always prioritize safety while complying with local regulations.
RCBOs for Electrical Safety in the Philippines
Ensuring electrical safety in the Philippines requires a thorough understanding of local standards and environmental conditions. Here is key information to consider when working with RCBOs in the country.
Electrical Standards in the Philippines
The standard household and commercial electricity in the Philippines operates at 220V and 60Hz, so make sure to choose RCBOs that are compatible with that voltage and frequency. When purchasing electrical components, it is essential to look for devices bearing the PS Mark or ICC sticker, which serves as assurance to the consumer that the products have been certified by the Bureau of Philippine Standards (BPS). These certifications also ensure compliance with relevant safety standards.
Climate and Environmental Considerations
The Philippines' high humidity and tropical climate present specific challenges for electrical systems, and excess moisture can increase the risk of earth faults. Therefore, it is crucial to ensure that any RCBO installed is rated for humid environments to prevent malfunctions. For outdoor or semi-exposed areas, using a device with an appropriate IP (Ingress Protection) rating is essential to protect it from moisture, dust, and other environmental factors.
Installation and Maintenance
Proper installation and maintenance are key to the functionality of any RCBO, so it’s imperative to ensure the device’s current rating matches the wire gauge and expected load of the circuit in a Philippine household or commercial installation. To comply with local regulations and ensure safety, always engage a PRC-licensed electrician for installation. Additionally, you should press the test button on the RCBO monthly to confirm it is functioning correctly and provides adequate protection.
Popular Brands
Eaton
Browse RCBOs from leading brand Eaton and discover the most suitable product for your requirements.
ABB
With a comprehensive range of products to choose from, RCBOs from ABB are a popular choice.
Schneider Electric
Schneider Electric has a wide range of different RCBOs on offer, with the full range available from RS.