• Published Oct 29, 2024
    • Last Modified Oct 29, 2024
  • 13 min

A Complete Overview of Cutters and Their Applications

Cutters Guide

In this extensive guide, we provide an in-depth exploration of different cutter types available today. From their unique characteristics to common sizes and practical applications, this article aims to equip you with the knowledge necessary to make informed decisions when choosing the right cutter for your upcoming projects.

What is a Cutter?

A cutter is a versatile hand tool designed for cutting a variety of materials, making it an essential instrument in numerous industries and applications. Typically, a cutter consists of two levers connected by a fulcrum, strategically positioned closer to one end. The shorter segment of the tool is known as the jaws, while the longer segment comprises the handles. This design leverages the principles of leverage, allowing users to exert significant force with minimal effort.

When the handles are pressed together, the gripping power is amplified and focused at the point where the jaws meet, enabling the cutter to slice through materials that may be too small or intricate to handle manually. This functionality makes cutters invaluable in tasks ranging from crafting and electronics to metalworking and construction. Cutters come in a wide array of types and sizes, each tailored for specific cutting tasks. The three primary categories of cutters include locking, adjustable, and non-adjustable models, with each type offering unique advantages based on the user's needs. Most cutters are constructed from durable materials such as steel, ensuring longevity and reliability during use.

Exploring the Various Types of Cutters

Cutters are indispensable hand tools widely used across multiple industries for cutting, trimming, and shaping a variety of materials. Below is an overview of various cutter types, highlighting their unique features and ideal applications.

Side Cutters

Side Cutters

Side cutters, also known as diagonal cutters or dikes, are designed to indent and wedge materials apart, offering a cleaner finish compared to traditional scissors or knives. These tools excel at cutting soft wires and leads but should be avoided on harder materials like nails or screws, as this can damage the cutting edges.

Ideal for:

  • Holding, splicing, or cutting leads
  • Stripping insulation from wires

Side cutters are essential for electricians and DIY enthusiasts alike, making them a staple in any toolbox.

Cable Cutters

Cable Cutters

Cable cutters are specifically engineered for electrical applications. These tools often feature insulated handles to protect against electrical shocks, making them crucial for safely cutting through thick cables without crushing the internal conductors.

Ideal for:

  • Electrical installations
  • Industrial applications

Cable cutters are particularly useful in environments where safety is paramount, ensuring that users can work confidently with electrical wiring.

Flush Cutters

Flush Cutters

Flush cutters are characterized by their angled and narrow pincers, allowing for precise cuts on soft and semi-hard metals. Their design ensures that the cutting edge sits flush against the material, making them perfect for trimming delicate components without leaving sharp edges.

Ideal for trimming:

  • Eyepins
  • Headpins
  • Beading wire

Flush cutters are commonly used in jewelry-making and other crafts where precision is key.

End Cutters

End Cutters

Also known as nippers, end cutters feature a nearly flat head that allows for cutting materials close to surfaces. This design is particularly useful for tasks requiring precision, such as cutting leads, springs, nails, and rivets.

Ideal for working with:

  • Leads
  • Springs
  • Nails
  • Bolts
  • Rivets

End cutters are invaluable in both construction and electrical work due to their ability to make clean cuts in tight spaces.

Diagonal Cutters

Diagonal Cutters

Diagonal cutters are designed to provide precise cuts at an angle, making them ideal for crimping and wedging cables apart. They are commonly used in electrical work, particularly for cutting soft copper or aluminum conductors.

Ideal for:

  • Gripping and cutting wires
  • Stripping insulation from cables

These versatile tools are essential for anyone working with electrical components or wiring.

Additional Types of Cutters

In addition to the main types of cutters mentioned above, there are several alternative models that cater to specific needs:

Wire Rope Cutters

Wire rope cutters are designed to pull the rope into their jaws, creating a clean cut without fraying. These tools are perfect for shearing wire rope and are commonly used in rigging and construction applications.

Bolt Cutters

Bolt cutters generate substantial torque, enabling them to cut through thick metal materials effortlessly. Their strength makes them a staple in the construction industry for tasks like snipping bolts off containers and cutting through heavy chains or leads.

Lineman's Cutters

Easily recognizable by their unique design, lineman's cutters have a shorter gripping surface and a cutting surface in the middle. They are favored in electrical and construction tasks for grasping, splicing, or chopping leads and stripping insulation.

Hydraulic Cutters

Hydraulic cutters feature a guillotine-style head that minimizes jams and can handle various materials, including wire ropes and solid bars. These tools are primarily used in power utility and electrical industries for cutting copper or aluminum power cables. Hydraulic models come in various versions, including manual and battery-operated options, catering to different user needs.

Bent Nose Cutters

Bent nose cutters are versatile pliers that can grasp, turn, and bend wires. Their flat jaws allow for gripping and twisting, making them essential in both electrical and mechanical applications. These tools come in various lengths to accommodate different tasks effectively.

From side cutters to hydraulic models, each type offers unique advantages tailored to different applications. Whether you're an electrician working on intricate wiring or a DIY enthusiast tackling home improvement projects, having the right cutter at your disposal is crucial for achieving precise results.

Diagonal Cutters vs Side Cutters

Diagonal cutters and side cutters are terms that are often used interchangeably, leading to confusion regarding their distinct features and applications. Both tools are designed for cutting wires and cables at an angle, utilizing a method that involves pressing and wedging the material apart rather than shearing like traditional scissors. This design makes them durable and suitable for demanding professional tasks. However, subtle differences between them can influence their effectiveness in specific situations.

Diagonal Cutters

Diagonal cutters, commonly referred to as diagonal pliers or dikes, are characterized by their angled cutting edges. This unique angle allows for precise cuts close to surfaces, making them ideal for delicate tasks where accuracy is crucial. Their compact and lightweight design enables users to handle them easily in tight spaces, which is particularly beneficial in electronics and jewelry making.

Key Features:

  • Precision Cutting: Diagonal cutters excel at cutting smaller wires, making them essential for intricate work.
  • Clean Cuts: They provide clean cuts without leaving sharp edges, which is vital for maintaining the integrity of electronic connections and preventing injuries in jewelry applications.
  • Versatility: Ideal for gripping and cutting soft copper or aluminum conductors, these tools are widely used in electrical work.

Ideal Uses:

  • Cutting small wires
  • Stripping insulation from cables
  • Working with delicate components in electronics and jewelry

Side Cutters

Side cutters, also known as side-cutting pliers, feature a blade that runs parallel to the handles. This design typically makes them more robust than diagonal cutters, allowing them to cut through larger and thicker materials effectively. Side cutters are often employed for general-purpose cutting tasks, including cutting aluminum and steel wires.

Key Features:

  • Greater Leverage: The design of side cutters provides increased leverage, making them advantageous when dealing with tougher materials.
  • Wider Jaws: The larger jaws enable side cutters to open wider, accommodating bigger items and enhancing their versatility across various applications.
  • Durability: Built to withstand heavy use, side cutters are ideal for construction and industrial tasks.

Ideal Uses:

  • Cutting larger wires
  • General-purpose cutting tasks
  • Snipping bolts or screws

The table below provides a clear and concise comparison of diagonal cutters and side cutters, highlighting their distinct features and applications.

Feature
Diagonal Cutters
Side Cutters
DesignAngled cutting edgesParallel cutting edges
Cutting AngleCuts at an angleCuts straight across
Best UseSmall, delicate tasksLarger, tougher materials
PrecisionHigh precision for fine cutsGood for general-purpose cutting
Jaw SizeCompact, smaller jawsWider jaws for larger items
LeverageLess leverage, suited for light workMore leverage, suited for heavy-duty work
Common ApplicationsElectronics, jewellery makingElectrical work, construction, metal cutting
DurabilityDurable but designed for finesseDurable and robust for tough tasks

Common Cutter Sizes

Cutters can be categorized based on either jaw length or overall tool length, with measurements typically expressed in millimeters (mm). The size of a cutter significantly influences its cutting capacity and the types of materials it can handle. Below, we explore some common cutter sizes and their ideal applications, helping you choose the right tool for your specific needs.

Diagonal Cutters

Diagonal cutters, also known as diagonal pliers or dikes, are widely used for cutting wires and small components. They come in several sizes, with standard options including 5", 6", 7", and 8". Among these, the 7" and 8" models are the most commonly used for general purposes.

  • 5" and 6" Sizes: These smaller sizes are ideal for light-duty tasks, such as cutting thin wires or performing intricate work in tight spaces.
  • 7" and 8" Sizes: Larger diagonal cutters provide more leverage, making them suitable for cutting thicker materials. When selecting a size, consider the material you will be cutting and the level of precision required.

Rotary Cutters

Rotary cutters are popular tools in quilting and sewing, available in four main sizes: 18mm, 28mm, 45mm, and 60mm.

  • 45mm Size: This is the most versatile option, suitable for a variety of cutting tasks, including fabric and quilting projects.
  • 28mm Size: Ideal for intricate patterns and tight curves, this size allows for precision cutting without damaging surrounding materials.
  • 60mm Size: Perfect for cutting through multiple layers of fabric or thicker materials, making it a favorite among professionals.

Choosing the right rotary cutter size depends on the type of material being cut and the complexity of the cuts needed.

Tenon Cutters

Tenon cutters are specialized tools used in woodworking to create precise joints. They range from 1/2" to 3" in size.

  • 1/2" and 3/4" Sizes: Smaller sizes are perfect for detailed projects like chair spindles or decorative elements.
  • 1 1/2" Size: This is the most popular choice for standard woodworking projects, balancing detail with structural integrity.
  • 2" and 3" Sizes: Larger tenon cutters are better suited for substantial projects like building swings or bunk beds.

Bolt Cutters

Bolt cutters are designed to cut through heavy materials like bolts and chains. They come in various sizes, with larger models offering more leverage and cutting capacity.

When selecting a bolt cutter, consider the thickness and hardness of the material you need to cut. Larger bolt cutters can handle tougher jobs with ease.

Heavy-Duty Wire Cutters

Heavy-Duty Wire Cutters

Heavy-duty wire cutters are designed for robust applications, capable of cutting through thick wires and cables with ease. These cutters often feature larger jaws and longer handles, providing the necessary leverage to tackle tough materials. They are ideal for industrial and construction settings where durability and strength are paramount.

View Range

Mini Side Cutters

Mini Side Cutters

Mini side cutters are compact tools perfect for precision tasks that require access to tight spaces. With smaller jaws and handles, these cutters are well-suited for electronics, jewellery making, and other delicate applications. Their compact size allows for detailed work without compromising control or accuracy.

View Range

Large Wire Cutters

Large Wire Cutters

Large wire cutters offer a balance between size and cutting capacity, making them versatile tools for a range of applications. They are particularly useful for cutting medium to large gauge wires and are commonly used in electrical work and general maintenance tasks. The extended handles provide additional leverage, reducing the effort required to make clean cuts.

View Range

Versatile Applications of Cutters

Cutters are versatile hand tools that find applications across a multitude of industries, including electrical work, jewelry making, and construction. Their ability to cut, trim, and shape various materials makes them indispensable for both professionals and DIY enthusiasts. Below, we explore the diverse uses of different types of cutters, highlighting their specific functionalities and ideal applications.

Cutting Wires

Side cutters, often referred to as diagonal cutters or dikes, are primarily used for cutting and stripping wires in electronic components. These specialized tools excel at safely removing insulation from wires without damaging the underlying conductors—a crucial process known as stripping. Proper wire stripping is vital as nicking the wire can lead to broken connections or electrical short circuits. While knives and scissors can perform this task, they pose a higher risk of damaging the copper wire. Using dedicated wire cutters ensures a clean cut and preserves the integrity of the wire, making them the preferred choice for electricians and hobbyists alike.

Cutting Nails and Screws

For cutting nails and screws, bolt cutters are the tool of choice. These heavy-duty cutters provide the necessary leverage to snip through tough materials effectively. To use bolt cutters efficiently, position the tool as close to the shank of the screw or nail as possible. If the fastener is too tight to reach the shank, simply snip off the head instead. Bolt cutters are particularly useful in construction and maintenance tasks where quick and efficient cutting is required.

Jewlery Making and Crafting

In the realm of jewelry making, specialized cutters such as flush cutters and wire cutters are essential. Flush cutters feature a unique design that allows for precision cuts while minimizing the risk of leaving sharp edges. This ensures a polished finish on delicate jewelry pieces. Wire cutters are also invaluable for trimming wires and components without causing damage.

Heavy-Duty Cutting Tasks

For more robust cutting tasks, hydraulic cutters are available. These powerful tools utilize hydraulic force to cut through thick cables, wire ropes, and solid bars with ease. Hydraulic cutters are commonly employed in the power utility and electrical industries where they efficiently handle large conductors and overhead lines.

Choosing the Right Cutter Size

Choosing the appropriate cutter size depends on the specific tasks you intend to perform. Here are some factors to consider:

  • Material Type: The hardness and thickness of the material you intend to cut significantly influence your choice of cutter size. For instance, cutting through thicker or harder materials necessitates larger cutters that offer better leverage. Larger cutters can handle tougher materials like steel or heavy-duty cables, while smaller cutters are more suited for delicate tasks involving softer materials.
  • Task Precision: When precision is paramount, such as in tasks involving small wires or intricate components, smaller cutters are preferable. They provide better control and access to confined spaces, allowing for accurate cuts without damaging surrounding materials. For example, flush cutters are ideal for jewelry making, where precision is essential.
  • User Comfort: User comfort is another important consideration when selecting a cutter size. The tool should match the user’s hand size and strength. Larger cutters may offer more leverage but can be cumbersome for users with smaller hands, leading to fatigue during extended use. It's essential to choose a cutter that feels comfortable in your grip to enhance productivity and reduce strain.
  • Cutting Capacity: Selecting a cutter with an appropriate cutting capacity is critical to ensure longevity and maintain sharpness. Always choose a cutter rated for a higher gauge than what you typically cut. For example, if you frequently cut 18 AWG wire, opt for a cutter rated for 16 AWG or lower. This extra capacity helps prevent wear and tear on the tool and ensures efficient cutting performance over time.

Safety Tips for Using Wire and Cable Cutters

Using cutters, especially in electrical and industrial contexts, requires attention to safety and technique to ensure both efficiency and protection from injury. Here are some essential tips and guidelines for using wire and cable cutters effectively:

  • Wear Protective Gear: Always wear safety goggles to protect your eyes from flying debris and particles. Cut-resistant gloves can also provide an extra layer of protection against accidental cuts or abrasions.
  • Proper Cutting Technique: Aim to cut at right angles to the material to ensure a clean cut and avoid damaging the tool. Avoid wiggling the cutter or bending the wire back and forth against the cutting edges, as this can dull the blade and compromise the cut.
  • Tool Selection: Use the appropriate tool for the task. Avoid using wire cutters on nuts and bolts; instead, use a wrench for these tasks. For hardened cables, ensure that the tool is specifically designed to handle such materials to prevent damage to the cutter.
  • Tool Maintenance: Regularly oil the hinge of your cutters with a drop of oil to maintain smooth operation. Ensure the cutting edges are sharp, as dull blades require more force, increasing the risk of injury and reducing the quality of the cut.
  • Avoid Excessive Force: Do not use excessive force when cutting, as this can lead to accidents. If a lot of force is needed, the blade might be dull, or the tool may not be suitable for the material.
  • Handle Design: Choose cutters with a grip span between 6cm and 9cm to prevent hand fatigue and avoid pinching your fingers when the tool is closed. Ensure the handles are comfortable and provide a secure grip.
  • Safety Precautions: Avoid using cushioned handles when working with electrical wiring, as they may not be insulated and could pose a risk of electrical shock. Keep cutters away from excessive heat to prevent damage to the tool.
  • Proper Storage: After use, store cutters in a safe place, away from children and in a location where they won't be accidentally used or damaged. Ensure the blade is retracted or covered when not in use.
  • Cutting Motion: When using pliers or cutters, apply pressure by pulling the tool towards you rather than pushing away. This technique reduces the risk of slipping and potential injury.

Related links

Be the first to know about our latest products and offers

Email address

The personal information you provide to us when signing up to this mailing list will be processed in line with the Privacy Policy