- Published Feb 21, 2024
- Last Modified Apr 4, 2024
- 6 min
Electric Motor Maintenance Tips to Ensure Its Longevity
Proper maintenance is important to ensure the longevity of your electric motor. Learn tips on how to conduct proper electric motor maintenance today.
![RS marketing banner](http://res.cloudinary.com/rspoc/image/upload/w_1248,h_180,c_crop,c_fill,f_auto,q_auto/dpr_auto/v1664363757/RS%20CONTENTFUL/Discovery/Hero%20Banners/001%20Generic%20Banner/SEO_Guide_Banner_New_Template_5120x360px.jpg)
![](http://media.rs-online.com/image/upload/w_620,h_413,c_crop,c_pad,b_white,f_auto,q_auto/dpr_auto/v1581356842/F0424150-01.jpg)
Electric motors are the heartbeat of various industries in the Philippines, driving economic growth and technological advancement. They are used in various industries, including oil and gas, automotive, manufacturing, and construction. However, the main users of electric motors are the manufacturing and construction industries, according to a study published in 6Wresearch.
The electric motor that is more commonly used by industries in the Philippines is the AC motor. This motor is used in a wide range of applications, including computers, HVAC systems, and conveyor systems. There has also been a rise in the DC motor segment due to the demand for more renewable energy systems and electric vehicles.
The widespread use of electric motors, both AC and DC motors, highlights their significance in the country's development and underscores the need for effective maintenance practices. They are an indispensable component of the machines we use today. Therefore, understanding the significance of their proper maintenance is essential for longevity and optimal performance. With this, we will delve into the essential aspects of electric motor maintenance and provide ways to prolong their life.
Why Is Preventive Maintenance of the Motor Important?
Regular preventive maintenance of your electric motor minimizes the risk of unexpected breakdowns and contributes to energy savings and reduced operational costs. Neglecting maintenance can lead to increased downtime, costly repairs, and a decline in overall productivity. That’s why a proactive and systematic approach to maintenance is essential to maximise the lifespan of electric motors.
Ways to Prolong the Life of Electric Motors
Here are some maintenance practices to increase the longevity of your electric motor:
1. Routine Maintenance
Routine inspections and meticulous cleaning are the cornerstone of effective electric motor maintenance. It's imperative to conduct regular examinations for any signs of wear, debris, or dirt so you can ensure optimal performance and optimal use of your electric motor.
For accumulated debris or dirt, adhere to a scheduled routine cleaning for your machine or appliance. Consistent cleaning practices prevent the build-up of contaminants, which could compromise the overall performance of your motor. Additionally, maintaining cleanliness in the surrounding area is paramount to reducing the risk of external contaminants entering the motor, ensuring smooth and uninterrupted operation.
If wear and tear issues are identified during routine inspections, it's advisable to seek professional assistance promptly. Having a certified professional assess the equipment can help address potential problems before they escalate, safeguarding your electric motor's overall performance and longevity. Proactive measures and timely interventions are key to ensuring the seamless operation of your motor over its extended lifespan.
2. Vibration Analysis
Excessive vibration is particularly a concern for AC motors, where it can be a mechanically and electrically destructive force. As such, vibration analysis tools, such as vibration meters, are invaluable for detecting misalignments, imbalance, and other issues that can lead to premature motor failure. Maintenance professionals can identify problems early by monitoring vibrations regularly and facilitating timely interventions. Addressing these issues right away can improve your electric motor's overall efficiency and lifespan.
3. Temperature Monitoring
Monitoring the temperature of your electric motor is a proactive maintenance approach to prevent it from overheating. Excessive heat can lead to insulation degradation, bearing failure, and other issues that shorten the motor's lifespan. There are many reasons why the motor will overheat, which include excessive load placed on the motor, poor power conditions, excessive stops and starts, and environmental influences.
![Lubricate Your AC & DC Motors](https://res.cloudinary.com/rspoc/image/upload/f_auto/q_auto/v1707875432/RS%20CONTENTFUL/Philippines/IDEA%20AND%20ADVICE/Electric%20Motor%20Maintenance%20Tips%20to%20Ensure%20Its%20Longevity/Blog_4_-_2.jpg)
4. Lubricate Your AC & DC Motors
Bearings are a common point of failure for electric motors due to poor lubrication practices. As such, proper lubrication of your AC or DC motors should be an essential part of your maintenance practice. The first step is to know which type of lubricant is appropriate for your electric motor. Factors to consider when choosing your lubricant are the horsepower of the electric motor, application, and ambient temperature.
For example, oil is the best type of lubricant for a gear motor that’s widely used in industrial applications. It is an optimal lubricant because it is free-flowing and constantly found on the surfaces of the teeth as the motor runs. On the other hand, grease is the best type of lubricant for smaller AC and DC gear motors as it is simple to apply and does not require visual lubrication inspections.
When lubricating your electric motor's bearings, ensure the manufacturer’s operating instructions and any additional instructions are followed. While lubrication is critical, excessive grease or oil can damage the motor.
5. Training and Education
Training and education are among the most effective ways to ensure the proper use and maintenance of electric motors. Educating your staff so they have the knowledge and skills required to operate and care for appliances with AC and DC motors enhances their understanding of the equipment. Well-trained personnel are more likely to follow best practices, minimizing the risk of human error and promoting a culture of proactive maintenance.
Keep Records
Maintaining detailed records of maintenance and inspection activities is essential for tracking the health and history of electric motors. Records help identify patterns, track performance trends, and effectively schedule preventive maintenance. Moreover, access to historical data facilitates informed decision-making for your staff and ensures that maintenance activities are tailored to the specific needs of each motor.
Find Electric Motors for a Wide Range of Applications
To secure high-quality electric motors, look no further than RS Phillippines. Our extensive catalog boasts various AC and DC motors from reputable manufacturers worldwide. Whether you require motors for industrial machinery or construction equipment, we ensure you have access to the necessary components. Trust RS Phillippines to provide the motors you need for optimal performance and longevity in your diverse applications.
Popular Electric Motor Brands
Panasonic
With a focus on precision engineering and technological innovation, Panasonic's AC motors are designed to deliver exceptional performance across a spectrum of applications. Whether for industrial machinery or consumer electronics, Panasonic's motors are characterized by reliability, efficiency, and longevity.
Schneider-Electric
Schneider-Electric DC motors are engineered to deliver precision and efficiency in various applications that demand precise control and variable speed operations.