- Published Mar 8, 2023
- Last Modified Jul 19, 2024
- 15 min
Transform Your DIY Game Using Our Essential Jigsaw Guide
Choose the ideal jigsaw for your needs using our in-depth guide on tool types, applications, and essential safety practices.
![](http://res.cloudinary.com/rspoc/image/upload/w_1248,h_180,c_crop,c_fill,f_auto,q_auto/dpr_auto/v1669301157/RS%20CONTENTFUL/Discovery/Hero%20Banners/Jigsaw%20Tools/SEO_Guide_Banner_5120x360px84Jigsaw_Tools.jpg)
Reviewed by Luqman Said Abdullah, Technical Support Engineer (March 2021)
What is a Jigsaw Tool?
A jigsaw is a versatile power tool that features a rapidly reciprocating blade, designed to make precise curved cuts and intricate patterns in various materials. This adaptable tool excels at creating both straight and curved cuts, making it indispensable for both DIY enthusiasts and professional craftsmen. Jigsaws are capable of cutting through a wide array of materials, from wood and plastic to metal and even certain masonry materials, making them a go-to choice for numerous projects.
Key Factors to Consider When Choosing a Jigsaw:
- Ergonomics and Handling: The way you prefer to hold and maneuver the saw is crucial. Consider the tool's weight, grip design, and balance to ensure comfortable operation during extended use.
- Cutting Settings and Features: Modern jigsaws offer a range of settings to optimize performance for different cutting applications. Look for features such as variable speed control, orbital action settings, and bevel cutting capabilities to enhance versatility.
- Blade Compatibility and Selection: The type of blade and its compatibility with the jigsaw are vital for achieving the desired results. Consider the variety of blades available for the tool, including those for different materials and cut types, as well as the ease of blade changing mechanisms.
- Power Source: Decide between corded models for consistent power or cordless options for enhanced portability. Each has its advantages depending on your typical work environment and project requirements.
- Dust Management: Some jigsaws come with built-in dust blowers or vacuum attachments, which can significantly improve visibility and cleanliness during operation.
- Additional Features: Look for extras like LED lights for improved cut-line visibility, laser guides for enhanced accuracy, and tool-less blade change systems for convenience.
Versatile Applications of Jigsaws
Jigsaws are highly versatile tools that offer several advantages over circular saw, particularly in terms of safety and precision. Their ability to make intricate cuts and handle a variety of materials makes them indispensable for numerous applications:
- Woodworking Projects: Jigsaws excel at cutting wooden sections, making them ideal for repurposing and upcycling projects. They can create both straight and curved cuts with ease.
- Angle Cutting: Many jigsaws feature adjustable baseplates, allowing for bevel cuts at various angles, typically up to 45 degrees.
- Precise Cutouts: Jigsaws are perfect for creating interior cutouts in materials, such as for electrical outlets or sink installations.
- Craft Projects: The tool's precision makes it suitable for intricate craft work, including stenciling and pattern cutting.
Materials Suitable for Jigsaw Cutting
Jigsaws can effectively cut through a wide range of materials, including:
- Wood (various types and thicknesses)
- Plastic (including acrylic and PVC)
- Metal (thin sheets and pipes)
- Ceramic tiles
- Laminate flooring
- Plywood and MDF
- Thin aluminum and other soft metals
Wood Cutting with Jigsaws
Jigsaws are particularly well-suited for cutting wood, making them a staple in many woodworking shops. However, the effectiveness of a jigsaw in cutting wood depends on several factors:
- Blade Length: Longer blades can cut thicker materials but may sacrifice some precision.
- Saw Base: A sturdy, flat base ensures smoother, more accurate cuts.
- Blade Teeth: The number of teeth per inch (TPI) and tooth pitch affect the cut quality and speed.
- Wood Hardness: Softer woods are easier to cut, while harder woods may require specialized blades.
- Motor Power: More powerful motors can handle thicker and harder materials more efficiently.
For optimal results, match the blade type to the specific wood and desired cut quality.
Cutting Tiles with Jigsaws
While not their primary function, jigsaws can indeed cut ceramic tiles when equipped with the right blade. Key points to consider:
- Blade Type: Use diamond-grit or carbide-grit blades specifically designed for tile cutting.
- Precision Work: Jigsaws are excellent for creating precise notches, cuts, and openings in tiles.
- Cooling: Ensure proper cooling of the blade to prevent overheating and damage.
- Safety: Wear appropriate safety gear, including eye protection and a dust mask.
Cutting PVC Pipe with Jigsaws
Jigsaws can effectively cut PVC pipes, but proper technique is crucial:
- Tool Selection: Use a high-powered jigsaw for best results.
- Secure the Pipe: Firmly clamp the PVC pipe to a stable work surface to prevent movement.
- Blade Choice: Select a blade with fine teeth designed for plastic or PVC cutting.
- Minimize Vibration: Use steady, even pressure to reduce vibration and prevent chipping.
- Safety Precautions: Wear safety glasses and follow all recommended safety guidelines.
By understanding these capabilities and techniques, you can maximize the utility of your jigsaw across a wide range of projects and materials.
Corded vs Cordless Jigsaws
When choosing a jigsaw, one of the primary considerations is the power source. Jigsaws come in two main types: corded and cordless. Each type has its own set of advantages and ideal use cases, catering to different needs and working environments.
Corded Jigsaws
Corded jigsaws are the go-to choice for tasks requiring sustained power and extended use. Here's what you need to know about these robust tools:
- Power Source: These jigsaws plug directly into standard 120V AC wall outlets or compatible power generators, ensuring a constant power supply.
- Performance: Ideal for cutting hard materials like thick hardwoods, metals, or dense composites due to their consistent power output.
- Motor Design: Equipped with electric motors that drive the reciprocating saw blade, providing reliable and steady performance.
- Durability: Generally more robust and able to withstand heavy-duty use over long periods.
- Cost-Effectiveness: Often less expensive than their cordless counterparts and don't require battery replacements.
- Limitations: The power cord can restrict mobility and may not be suitable for job sites without readily available power sources.
Cordless Jigsaws
Cordless jigsaws offer unparalleled convenience and portability, making them excellent for various applications:
- Power Source: Operate on rechargeable lithium-ion batteries, typically ranging from 18V to 36V, with higher voltages generally providing more power.
- Portability: Ideal for job sites without easy access to power outlets or for working in tight, hard-to-reach spaces.
- Safety: Eliminate the risk of tripping over power cords, enhancing workplace safety.
- Versatility: Excel at precise cutting tasks, including intricate curves and interior cutouts in various materials, especially wood.
- Battery Life: Modern lithium-ion batteries offer improved run times, but consider having spare batteries for extended use.
- Performance Variability: Power output may decrease as the battery depletes, potentially affecting cutting performance on harder materials.
- Weight Considerations: While free from cords, the battery can add weight to the tool, which may impact user fatigue during prolonged use.
- Technological Advancements: Many cordless models now feature brushless motors for increased efficiency and longer tool life.
How to Use a Jigsaw
Using a jigsaw effectively requires proper technique, safety awareness, and an understanding of the tool's capabilities. This guide will walk you through the essential steps to ensure safe and precise cutting with your jigsaw.
Safety First: Preparing for Your Cut
Before you begin, it's crucial to prioritize safety. Always wear appropriate personal protective equipment (PPE) including safety goggles, a face mask, and work gloves. Hearing protection is also recommended for prolonged use. Ensure you have the correct blade fitted for your specific cutting application - the suitability of the blade may be specified on the packaging or label.
Prepare your workspace by:
- Securely clamping your workpiece to a stable surface
- Ensuring the cutting area doesn't extend beyond the edges of the work surface
- Clearing the area of any potential obstacles or trip hazards
Setting Up for Precision
Accurate marking is key to achieving precise cuts. Whether you're cutting straight lines or curves, take extra care when drawing your cutting line. This line will guide your cut and help prevent overcutting. For curved cuts, consider using templates or stencils for greater accuracy.
Adjust your jigsaw settings according to your cutting needs:
- Set the orbital action appropriate for your material
- Adjust the speed setting (lower for metals and precise cuts, higher for wood and straight cuts)
- Set the bevel angle if making angled cuts
Executing the Cut
When you're ready to begin cutting, firmly grip the jigsaw's handle and position the base plate flat against the workpiece. Squeeze the trigger and allow the blade to reach full speed before making contact with the material. Guide the saw along your marked line, applying steady, even pressure. For curved cuts, use gentle pressure to steer the blade along the curve.
Pay attention to the saw's performance as you cut:
- Adjust cutting speed if you encounter resistance or kickback
- Maintain a consistent pace; don't force the saw through the material
- For thicker materials, consider making multiple passes, gradually increasing depth
Continue cutting until you reach the end of your marked line. Keep the saw running until the blade has fully exited the material, ensuring cut-off pieces fall away safely without contacting the blade or power cord.
Post-Cut Procedures and Maintenance
After completing your cut, allow the blade to come to a complete stop before setting the tool down. Use sandpaper or a file to smooth any rough edges left by the cut. Clean up any sawdust or debris from your workspace to maintain a safe environment.
To keep your jigsaw in top condition:
- Unplug the tool (or remove the battery for cordless models) after use
- Clean the jigsaw, paying particular attention to ventilation slots
- Store the tool in a dry, secure location
Jigsaw Blades
The jigsaw itself is just one part of the equation – selecting high-quality blades that suit your specific needs is equally crucial. With the wide variety of jigsaw blades available from leading manufacturers, choosing the right one can be challenging. When selecting a blade, consider both the material you'll be cutting and the type of cut you need to make.
Types of Jigsaw Blades
Jigsaw blades come in various types, each designed for specific applications. The blade type affects both the cutting speed and the finish quality of your work. Blades can be categorized by their shank type, tooth count, material composition, or suitability for specific materials.Common jigsaw blade varieties include:
- T-shank blades: The most common and compatible with most modern jigsaws
- U-shank blades (Universal): Less popular now, but still used in some older models
While multi-purpose blades offer affordability and convenience, specialized blades often provide superior results for specific materials.
Blade Material Types
The blade's material significantly impacts its durability and suitability for different applications. Choosing the right material ensures you're using the best blade for your project.Common blade materials include:
- High carbon steel: Affordable and flexible, ideal for wood cutting
- High-speed steel: Durable and heat-resistant, suitable for metal, plastic, and wood
- Bimetal: Highly durable, primarily used for heavy-duty metal cutting
- Tungsten carbide: Extremely heat-resistant and durable, ideal for ceramics and stainless steel
Blade Lifespan and Maintenance
The lifespan of a jigsaw blade depends on various factors, including power settings and the materials being cut. All blades will eventually wear down and lose their cutting ability with repeated use. To extend blade life:
- Sharpen blades before fitting
- Avoid forcing the jigsaw if you encounter cutting resistance
- Replace blades when you notice a significant difference in cutting performance
Changing a Jigsaw Blade
Proper blade changing technique is essential for both safety and tool longevity. Follow these steps:
- Ensure the blade has cooled and remove the battery (for cordless models)
- Locate the spring-loaded lock at the top of the jigsaw
- Position the lock parallel to the blade guide
- Carefully insert the new blade
- Release the lock and gently tug the blade to ensure it's secure
When removing a blade:
- Allow it to cool completely
- Remove the battery or unplug the tool
- Push the spring-loaded lock up to release the blade
Jigsaw Spotlight
In this video, we take an in-depth look at the 240V Bosch PST Universal+ Corded Jigsaw, a versatile power tool designed to meet a wide range of cutting needs. This comprehensive overview showcases the jigsaw's core features and demonstrates its diverse applications, making it an essential watch for both DIY enthusiasts and professional craftsmen.
Choosing the Right Jigsaw
Selecting the perfect jigsaw involves considering various factors to ensure it meets your specific needs. Your decision should be based on the frequency of use, the type of projects you'll undertake, and your personal preferences. Let's explore the key aspects to consider when choosing a jigsaw.
Jigsaw Stroke Length
- Defines the vertical distance covered by the blade during cutting
- Longer stroke length generally means higher cutting efficiency
- Suitable for a wider range of materials
Jigsaw Power
- For corded models, look for motor power over 500W for most tasks
- Heavy-duty users should consider jigsaws with over 700W
- Cordless jigsaw power is measured in volts (typically 18V or 20V)
Jigsaw Speed
The cutting speed determines the materials the jigsaw can effectively cut:
- Slow (500-1,000 SPM): Ideal for ceramics, wall tiles, and glass
- Medium (1,500-2,000 SPM): Suitable for plastics and non-ferrous materials
- Fast (over 2,000 SPM): Best for wood cutting
Additional Features to Consider:
- Orbital action settings for more aggressive cutting in wood
- Dust blower or vacuum attachment for cleaner work
- LED light for improved visibility
- Tool-less blade change mechanism for convenience
Remember, the best jigsaw for you is one that balances power, precision, and comfort for your specific needs. Whether you're a DIY enthusiast or a professional woodworker, taking the time to choose the right jigsaw will ensure better results and a more enjoyable woodworking experience.
Popular Brands
Bosch, DeWALT, and Makita jigsaws are among the most popular brands. Bosch jig saws are used across Europe and have a great reputation for reliability. DeWALT jigsaws are also of good quality and suitable for a range of tasks. Makita jig saw blades and tools are popular among professionals, with many models offering advanced functionality.
Some of the key benefits and applications for each brand's tools are listed in the content below: