- Published May 31, 2024
- Last Modified Nov 11, 2026
- 13 min
A Complete Guide to Gate Valves
A gate valve is a linear isolation valve that starts or stops the flow of fluid through a pipeline by raising or lowering a wedge-shaped, parallel, or knife-edge gate into the flow path. Widely used across industrial, commercial, and plumbing applications, gate valves provide full shut-off when closed and minimal pressure loss when fully open. This guide explains what a gate valve is, the main gate valve parts, how gate valves work, common gate valve types, and typical gate valve applications.


What Is a Gate Valve?
A gate valve is an isolation valve used to start or stop the flow of liquid, steam, or gas through a section of pipeline. Also called a sluice valve, it works by raising or lowering a gate into the flow path, allowing users to isolate a section of pipe when required.
Gate valves are generally bidirectional in most standard applications, meaning they can block flow from either direction when fully closed, subject to the valve design and service conditions.
They are a common linear-motion valve found in pipelines both above and below ground and typically consist of a valve body, bonnet assembly, gate, seats, stem, stem sealing arrangement, and a handwheel or actuator used for opening and closing the gate.
The primary purpose of a gate valve is to provide full isolation of process media. Advantages include complete shut-off capability for maintenance, troubleshooting, and system isolation, along with minimal pressure loss when fully open because the gate is withdrawn from the flow path. Gate valves are widely used due to their relatively simple design and suitability for a broad range of sizes and materials.
One limitation is that gate valves are not especially quick to open or close, because the handwheel requires multiple turns to raise or lower the gate fully. They are also not designed to throttle or control flow by being partially opened. Leaving a gate valve in a partially raised position can cause excessive vibration and may damage the gate or seats over time.
Gate Valve Parts
Every gate valve is built from a set of core components that work together to control flow. The main gate valve parts include the body, bonnet, gate, seats, stem, packing and gland, and the handwheel or actuator.

This is a cut-out diagram showing typical parts of a gate valve, giving a visual indication of its construction and operating mechanism. Key parts such as the bonnet, stem, seats, sealing components, and valve body are typically labelled for identification.
Body
The body is the main pressure-containing component of the valve. It connects to the pipeline through threaded, flanged, socket-weld, or butt-weld connections and houses the internal components, including the gate and seat assemblies.
Bonnet
The bonnet covers the opening at the top of the valve body and provides a pressure boundary around the stem. It can be removed to access the gate, seats, and other internal parts for inspection or maintenance.
Gate (Wedge or Disc)
The gate is the movable barrier that blocks or allows flow through the valve. Depending on the design, it may be a solid wedge, flexible wedge, split wedge, parallel slide gate, or knife gate.
Seat
The seats are the sealing surfaces inside the body that the gate presses against when closed. Most gate valves have two seats, one on each side of the gate, to form a tight seal and prevent leakage.
Stem
The stem transmits motion from the handwheel or actuator to the gate. Depending on the design, the stem may either rise visibly during operation (rising stem) or remain within the valve envelope (non-rising stem).
Packing and Gland
The packing is a sealing material fitted around the stem inside the bonnet to prevent fluid from leaking along the stem. The gland compresses the packing to maintain a secure seal.
Handwheel or Actuator
The handwheel is the manual control used to open or close the valve. In automated systems, the handwheel may be replaced by an electric, pneumatic, or hydraulic actuator for remote or programmed operation.
How Does a Gate Valve Work?

Understanding how gate valves work helps explain why they are used primarily for isolation duties.
Gate valves operate by moving a gate perpendicular to the flow path. When opened, the gate is raised completely out of the flow stream, creating a near full-bore flow path with minimal flow restriction. When closed, the gate moves downward until it contacts the valve seats and isolates the pipeline.
The handwheel rotates the stem, converting rotational motion into linear movement of the gate. In manually operated designs, turning the handwheel clockwise generally closes the valve while turning it counterclockwise opens it, although users should always follow manufacturer markings.
Gate valves may be supplied with rising-stem or non-rising stem designs. They are typically made out of brass, bronze, cast iron, ductile iron, carbon steel, and stainless steel, depending on the fluid, pressure, and environmental conditions.
Gate Valve Types
There are several types of gate valves, each designed for different operating conditions and pipeline requirements. The main distinctions relate to the shape of the gate, the stem design, and the connection method. Below is an overview of the most widely used gate valve types.
Wedge Gate Valves
A wedge gate valve is one of the most widely used gate valve types. The gate is slightly tapered, creating a wedging action against the seats when closed.
Subtypes include:
- Solid wedge gate valves
- Flexible wedge gate valves
- Split wedge gate valves
Solid wedge gate valves offer simple construction and good mechanical strength.
Flexible wedge valves incorporate a machined cut in the gate, allowing slight flexibility that helps compensate for thermal expansion and reduces the likelihood of thermal binding.
Split wedge valves use a two-piece gate arrangement that can better accommodate seat alignment and thermal variations.
Parallel Gate Valves
A parallel gate valve uses parallel sealing surfaces rather than a tapered wedge arrangement. Unlike wedge designs, the sealing force comes from line pressure pushing the downstream disc against its seat rather than from mechanical wedging. Parallel-slide designs are commonly used in certain high-pressure and high-temperature applications, where thermal expansion could affect wedge-type valves.
Knife Gate Valves
A knife gate valve is primarily designed for slurries, pulp, wastewater, and media containing suspended solids. The gate features a sharpened lower edge at the bottom, allowing it to cut through fibrous or viscous material during closure. This design makes knife gate valves an ideal choice in mining, wastewater treatment, and pulp-and-paper processing.
Rising Stem and Non-Rising Stem Gate Valves
Gate valves are available in rising stem and non-rising stem configurations. On a rising stem valve, the stem moves upward as the gate opens, providing a visible indication of valve position. This design is common in above-ground installations where operators need to confirm at a glance whether the valve is open or closed. Non-rising stem valves keep the stem enclosed within the body, with the gate traveling along internal threads. These are better suited to underground or space-restricted installations where vertical clearance is limited.
Flanged Gate Valves
A flanged gate valve uses bolted flanges to connect the valve body to the pipeline rather than threaded or welded joints. Flanged connections allow for easier installation and removal, making them the choice for systems that require periodic maintenance. They are widely used in industrial process systems, water infrastructure, and larger pipe sizes, and are better suited to higher-pressure applications than screwed connections.
How to Select a Gate Valve
Selecting the right gate valve depends on the process fluid, operating conditions, and installation requirements. While the basic gate valve function remains the same across designs, factors such as pressure rating, material compatibility, and connection type can significantly affect performance and service life.
When choosing a gate valve, consider the following factors:
Pressure and Temperature Ratings
Gate valves must be suitable for the maximum operating pressure and temperature of the system. Industrial gate valves are commonly specified using pressure ratings such as:
- PN10, PN16, PN25, and PN40 (metric pressure ratings)
- ASME Class 150, 300, 600, and higher (imperial pressure classes)
Always verify that the gate valve's pressure-temperature rating matches the intended operating conditions in order for it to function as intended.
Valve Material
The valve body and internal materials should be compatible with the process media:
- Brass gate valves are commonly used for domestic water, plumbing, and HVAC systems.
- Bronze gate valves offer good corrosion resistance for water and marine applications.
- Cast iron gate valves are commonly used in water distribution systems.
- Ductile iron gate valves provide greater strength and impact resistance than cast iron.
- Carbon steel gate valves are widely used in industrial process systems.
- Stainless steel gate valves offer excellent corrosion resistance and are frequently specified for aggressive media, food processing, and chemical applications.
End Connections
Gate valves are available with several connection types:
- Threaded (screwed)
- Flanged
- Socket-weld
- Butt-weld
The appropriate connection depends on pipe size, pressure requirements, and maintenance considerations.
Manual or Actuated Operation
While many gate valves use handwheel operation, electrically actuated, pneumatic, and hydraulic versions are available where automatic or remote control is required.
What Are Gate Valves Used For?
Gate valves are used for starting or stopping the flow of liquid, steam, or gas through a pipeline. Their primary purpose is full isolation: they deliver unrestricted flow when fully open and a complete seal when fully closed. This makes them one of the best valve types for applications that require reliable shut-off without significant pressure loss.
Common gate valve uses and applications span a wide range of industries, including:
- Water distribution systems
- Wastewater treatment facilities
- Oil and gas processing
- Petrochemical plantsPower generation facilities
- HVAC systems
- Building services
- Industrial process plants
- Marine and offshore systems
- Fire protection water systems
Certain gate valve types are suitable for both high-pressure and high-temperature service, provided their pressure-temperature ratings and material specifications are appropriate for the application. Gate valves are also frequently installed on residential and commercial water supply lines, where their full-bore design allows unobstructed flow and easy maintenance of downstream pipes and fittings.
Unlike some other shut-off valves, a gate valve is intended to be used only in its fully open or fully closed position. Leaving it partially raised will not effectively control the flow rate and may cause excessive vibration, risking damage to the gate and seats. For applications that require flow regulation rather than full isolation, other valve types such as globe valves or float valves may be more appropriate.
Gate Valves vs Other Valve Types
Gate valves are one of several isolation and control valve types used in pipeline systems. Understanding how they compare to other common designs can help you select the right gate valve or alternative for a given application.
Gate Valve vs Ball Valve
A ball valve uses a rotating ball with a bore to control flow, whereas a gate valve uses a linear-moving gate. Ball valves require only a quarter-turn to open or close, making them faster to operate. Gate valves take multiple turns but may offer a tighter seal in larger pipe sizes. The choice between the two typically depends on the pipe size, the medium, and how frequently the valve needs to be operated.
Gate Valve vs Check Valve
A check valve allows unhindered flow in one direction while preventing backflow in the opposite direction. It operates automatically, without a handwheel or actuator. Gate valves, by contrast, are bidirectional and require manual or automated actuation to open or close. The two serve different purposes: gate valves provide deliberate, full shut-off, while check valves guard against reverse flow. For a deeper look at check valve designs and applications, see our check valves guide.
Gate Valve vs Butterfly Valve
A butterfly valve uses a disc that rotates on a central axis to control flow. Like ball valves, butterfly valves require only a quarter-turn to operate, so they are faster to open and close than gate valves. They are also more compact, making them useful where space is limited. However, gate valves generally provide a tighter seal and are better suited to applications where zero leakage is critical. Some butterfly valve designs do allow throttling, which gate valves cannot safely provide.
Gate Valve vs Globe Valve
A globe valve is designed for flow regulation and throttling, not just on/off isolation. Its disc moves perpendicular to the flow path and can be held at intermediate positions to control flow rate precisely. Gate valves are strictly for full-open or full-closed service. Where an application requires both isolation and flow control, a globe valve may be the better choice, while a gate valve is preferred when the priority is unrestricted, full-bore flow with minimal pressure drop.
How to Use a Gate Valve
Gate valve operation is simple, only requiring the user to turn the handwheel in the correct direction to open or close the valve as necessary. Closing or opening a gate valve involves rotating the wheel through 360 degrees in the required direction. This, in turn, rotates the threaded valve stem and raises or lowers the attached gate disk.
How to Tell If a Gate Valve Is Open or Closed
On a rising stem valve, the stem position provides a visible indication of whether the gate is open or closed. When the stem extends above the bonnet, the valve is open; when it sits flush, the valve is closed. Determining valve position can be more difficult than with quarter-turn valves such as ball valves and butterfly valves. For most gate valves:
- Clockwise rotation closes the valve.
- Anti-clockwise rotation opens the valve.
While these directions are generally applicable across a wide range of gate valves. Manufacturer markings should always be followed.
Unless you know for a fact that a gate valve is jammed or bound, you should always stop turning when you start to feel significant resistance. Continuing to turn a gate valve against resistance can damage the valve, or the pipes and fittings it is installed on. It may therefore be necessary to try turning a gate valve in either direction to ascertain which position it is currently in.
Gate Valve Maintenance Considerations
Routine inspection and maintenance can help maximize gate valve service life, reduce the risk of leakage or operational issues, and maintain optimal function.
Common maintenance considerations include:
- Inspecting the stem, packing, and gland for signs of leakage.
- Exercising infrequently used valves periodically to prevent seizure.
- Checking operating torque for signs of corrosion or internal wear.
- Inspecting flange connections and body seals where accessible.
- Replacing worn stem packing when leakage develops around the stem assembly.
Gate Valve FAQs
Recommended Brands for Gate Valves
Sferaco
Sferaco manufactures gate valves in brass and stainless steel for industrial and commercial use. Their range covers a variety of sizes and connection types suited to demanding service environments.
Conex-Banninger
Conex-Banninger produces a range of brass and copper-alloy gate valves for plumbing and HVAC systems. Their valves are designed for dependable shut-off in residential and commercial water supply lines.
Pegler Yorkshire
Pegler Yorkshire is a well-established name in pipeline fittings, known for sturdy construction and consistent performance. Their gate valves are widely specified across water, heating and general plumbing applications.
RS PRO
RS PRO is the in-house brand from RS Components, offering gate valves that meet exacting quality standards at a competitive price point. The range includes options in brass and other durable materials for a variety of pipeline applications.
Further Readings
Related links
- Understanding PID Temperature Controllers and Their Uses
- Comprehensive Guide to PTFE Tape and Its Applications
- The Ultimate Guide to Understanding Cable Glands
- A Complete Guide to Anemometers
- A Complete Guide to Pipe Cutters
- Understanding Epoxy Resin and Its Uses
- Understanding Shunt Resistors in Electrical Circuits
- Sprocket Essentials: From Basics to Advanced Tips